Since the failure rate of the servo amplifiers is very small, a line protection is sufficient from cost perspective. Further cost saving can be reached by group protection concept. If however a selective protection of the power supply is required…
Hi,
I have a customer who wanted to buy everything from Kollmorgen including the 24Vdc power supplies for logic, my understanding is that is about the only thing you do not offer unless I missed it somewhere? I did see 24V AKT modules but…
Valid for AKM, AKMH, AKD, S300, S700
Power supply for the feedback and signal evaluation of the two wire SFD3 and Hiperface DSL feedback systems require an electronic, which is built into the drive itself (AKD-N only) or into special…
Requirements to fusing of lines and devices are different for CE and UL/cUL regions.
Fuse types
Fuses - Operation in UL-cUL regions
Fuses - Operation in CE regions
Protection in case of groups, parallel topology
Building Power Supply…