Bring Logistics minimizes operational costs with automated VNA trucks.
SITI-B&T provides an AGV system for automated trolley handling.
An international primary metal manufacturer uses Automated Guided Vehicles (AGVs) in a new plant to move heavy loads in a high temperature environment.
V-TAB uses AGVs to minimize damage to paper rolls.
StoVerotec have minimized their internal transportation costs by automating the transportation of polystyrene blocks from the production area to the warehouse.
With the “Titan” series, Bottero Group developed a fully automated plant for glass processing that performs bilateral grinding of pane edges.
Kuka's compact robots in the KR Agilus series are precise, agile and fast. As agile systems these five-axis and six-axis handling units feature short cycle times and high repeatability, particularly for pick-and-place tasks. Synchronous servo motors…
Challenge: Expand the functionality of pharmaceutical packaging machines to support new requirements that demand a reliable vision system.Solution: Robust direct drive technology using KBM that integrates an automated visual inspection process into…
450 Blisters per Minute
PLC, motion control, drive as one unit: A complete solution for PG Express
DIRECT DRIVES IN LASER CUTTING MACHINES
Cutting-edge laser machining
Latest machine-generation with cost-efficient mechanical transmission designs
A comparison of decentralized and centralized servo technology
Centralized or Decentralized? - Which architecture type delivers the best technical and commercial advantages?
The use of direct drive servo technology represents only one of the advantage points for the optimization of the screen printing machine which Kollmorgen worked on from its earliest stages of development.