Commutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases. If the rotor position of the motor is not determined correctly or the…
Commutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases. If the rotor position of the motor is not determined correctly or the…
So here's my story. Boss decided I'm going to start programming our custom built machines. He said," Theres a computer over there, go use it."
We use TRIO with Motion Perfect v4, Proface HMIs with GP-PRO EX, Kollmorgen drives and servos (at…
Hi, Kollmorgen team
I'm planning to use AKD and Zettlex Biss-C feedback sensor together.
WorkBench shows Biss-C renishaw on the feedback selection screen. Is it compatible only with Renishaw's BISS-C sensor?
I am…
DBL / DBK with Encoder
Feedback has no defined commutation offset. The commutation offset is determined with the help of the servo amplifier and stored in the encoder memory.
AKM with Hiperface encoder
Encoder is installed…
BiSS-C is a digital encoder protocol that permits a wide range of possible formats. The AKD supports the most common BiSS-C format, and can only guarantee support for the encoders listed in "Documented BiSS-C Encoders". To determine if a BiSS-C…
In October 2016, an inter-compatibility test was performed together with the company Heidenhain. In this event, the AKD was tested successfully with various types of Heidenhain Endat 2.2 encoders.
The devices tested can be found in this…