So here's my story. Boss decided I'm going to start programming our custom built machines. He said," Theres a computer over there, go use it."
We use TRIO with Motion Perfect v4, Proface HMIs with GP-PRO EX, Kollmorgen drives and servos (at…
Hi.
One of our customers has F503 fault.
Following is the customer's environment.
Drive : AKD-x01207
Motor : AKM53L
Input Voltage : VBUS 640
It happens more than 5200RPM,
It doesn't happen less than 5000RPM(Current…
Method 1: Add CPS.Control Object 3000 to the PDO mappings
Example:
Then map the Object to a Dictionary variable in the project. Example below shows mapping CPS.Controls to a PLC variable named CPSControl
Hello.
We tried incremental with hall on S200 Drive to check if it has encoder fault
, such as removing encoder signal line, removing connector and removing encoder header.
When we tried removing encoders, except hall sensor, it has no…
This strange fault seems to happen after doing some AKD Modbus Dynamic Mapping. I could not find this type of fault anywhere in the documentation or on the KDN. Any ideas on what this might be?
The three horizontal lines are…
The command for clearing the fault history on the Servostar S300, S600, and S700 drives is CLREEPROM FLTHIST. That is a space between the two words. Type it into the terminal command line and press enter. Sometimes it is…