When logging to the SD card in KAS the SD card needs to be mounted. At what time or when does it ever need to be unmounted? If I were to mount it initially can I just leave it mounted?
The program calculates the pulses from the secondary FB each scan and and adds to the parameter: A1_X9EncIn. The reason that the calculations are needed in KAS is because the 2nd feedback that comes through Ethercat changes 0 to 2^31…