In the IDE project , the way to read/write an AKD analog or digital IO is to first link a variable in the dictionary to the I/O point as follows:
- Go to the AKD drive item in the EtherCAT section of the project…
This Article contains four videos that continue the KAS IDE Introduction series. The first two videos introduce the Function Block Library and the Control Panel, and the last two go step by step how to complete the third exercise that is attached as…
If you get this type of message (Missing MSVCR100.dll file ) when installing and starting up the KAS IDE on a PC with a Win7 operating system go to the internet and download the MSVCR100.dll file. Here is the link:…
Attached are a number of template programs for the KAS IDE for 1, 4, and 6 axes. They are extensions of the 2 Axis demo projects for the Structured Text, Ladder Diagram, and Sequential Function Chart programming languages that are included in the KAS…
The following procedure outlines setting up Modbus RTU communications between the AKI HMI and a third party device. With a Modbus TCP/IP connection between the PxMM and the same AKI HMI this configuration allows data to be transferred between…
The udpSendToVar and udpRcvFromVar functions (starting in soon to be released KAS version 2.11)can be use to read and write variables via UDP to and from a PxMM. The other device can be a PDMM or a third party device. In this example, for…