There are a number of KDN articles that contain videos, application notes, and demo programs to teach new users or refresh experienced users how certain features work. Below are links to these articles separated into sections based on the type…
This video introduces the KAS IDE, ST (Structured Text) Editor
Covered in the Video:
Syntax
Compile, run, and animation
Comments
Using Function and Function Blocks
Conditional Statements
Shortcut keys
(Reference to) Debugging
New Features
EtherCAT Diagnostics with:
Web-server tab with network topology
Functions/FBs for application program
Configurable Working Counter limit in the IDE
New HMIs: X2 Panel Models
New KVB v2.20 software
New function:…
Below are three embedded videos showing different features of the FFLD or Free Form Ladder Diagram editor in the KAS IDE software that can be used to write PLC code.
The first video shows shows how you can organize your code into separate networks,…
Below is a video showing the steps to create a new PLCopen axis in the KAS IDE. First you will add an axis by right clicking the PLCopen section in the Project Explorer. After giving the new axis a name, you can open a pop-up window to modify the…
Hardware Revision
Firmware Version
Date
Remarks
DB
1.6
30.05.2012
Starting version, incl. AKD HWR D and PDMM HWR B
EB
1.13.0 and later
2014-12
Hardware revision for export classification traceability…