Implementation of STO Inputs
There are two types of STO input in common use today:
DC-DC Type: isolated STO input based on using a DC-DC converter to power the date driver circuitry.
O-C Type: opto-isolated input of a drive that acts upon…
This article provides a detailed description of using the KSM Safety PLC with AKD Functional Safety Safe Stop. The Safe Stop operation involves the AKD performing a Controlled Stop function, disabling the output stage. The Safety PLC…
New Features
FailSafe over EtherCAT (FSoE) "Black Channel" Communication
AKD2G Drive Integration:
Backup/Restore
AKD2G with SMM options #2 (basic) and #3 (advanced)
Robotic Kinematic Transforms: T-Bot, H-Bot, and Gantry
IDE…
This article will help you understand the differences between older S700 (S701-724) drives with single-channel STO and newer dual-channel STO S700 drives.