'-------------- Device Params -----------------------
Params
End Params
'-------------- Define (dim) Global Variables --------
Dim indexdistance as integer
Dim homefound as integer
'-------------- Device Params -----------------------
Params
End Params
'-------------- Define (dim) Global Variables --------
Dim homefound as integer
Dim targetposition as integer
Dim speed as integer 'speed of initial move to sprayposition
Dim…
For KAS applications:
- using the PLCopen Motion engine
- with a total travel range of 1 revolution
- that use a SFD single turn absolute position feedback…
Kollmorgen Visualization Builder (KVB) software contains built in System Tags that give users access to information generated in the panel, and has a C# scripting engine that allows them to add custom logic.
Homing in the AKD Basic must be written into the program. You can program the homing sequence to do whatever you want it to do. In this example, it is homing to a mechanical hard stop. It lowers the current limits to prevent…
The AKD Basic drive does not have a homing procedure like the other AKD drive models. The homing procedure must be written into the Basic program. Here is one example of using the Position Capture feature to find the home position.…
In a KAS project, the following outlines reading a thermocouple temperature in units of 0.1 Degrees C from a AKT-AN-200 or AKT-AN-400 slice I/O module. Note: Reading this note will help you get started working through other AKT thermocouple…
The attached demo project shows how to control a servo axis with a KAS controller in Torque Mode instead fo the default Position Mode. This project requires a 2.9 release of KAS software and PDMM firmware, which is currently only available in beta…