The attached is a sample.kas project and video showing the PDMM running a 2 axis T-bot mechanism. The T-bot control algorithm was created by adding additional virtual axes to the project and using them in a…
The Function Block GetCtrlPerf allows the user to monitor KAS cpu loading in the application program and then take the application specific appropriate action if a limit is exceeded. Multiple outputs allow the user to select the output that fits the…
This is a sample program of a rotary knife application. I didn't get a chance to test it in the field, just at my desk. The idea is the program will use operator input to create a cam profile, execute the profile, and correct the knife…
'-------------- Device Params -----------------------
Params
End Params
'-------------- Define (dim) Global Variables --------
Dim indexdistance as integer
Dim indexspeed as integer
Dim jogspeed as integer
Dim starthome as integer
Dim startmove as…