Attached is an example Visual Basic Telnet communications program to talk to the AKD. No warranties or support but this program is so simple, I'm not sure it needs much support.
When debugging a program in KAS, you may run into a situation where there is a division by zero. These errors can be challenging to locate. The solution is to have an exception routine for this condition. Adding a breakpoint in your exception handler…
KAS has a HTTP communication option for users to write their own programs (in C++, C#, JAVA, visual basic, etc) and be able to read or write any variable in a KAS project. It is documented in the 2.8 software, and I have attached a demo program…
Attached is a demo program showing an example of how to use cam creation function blocks to build a completely new profile while a program is running. The main function required is MLProfileBuild located in the function block library under…
When using Kollmorgen HMIs with KAS Controllers, modbus addressing is done automatically to save programming time and ensure everything is mapped correctly. When using third party HMIs or other Modbus devices, can use our separate Fieldbus…
This KAS project contains a PLCopen program meant to be used with our 2 Axis PDMM Demo hardware. Inside it also has a KVB project for our 7 in CDA HMI panel to control everything and show off advanced features such as recipe handling,…