DEVICENET HOME COMPLETE – S300
The S300 does not support this command. Page 96 give a summary of DeviceNet features not supported with the
SERVOSTAR 300. This shows that the Position Controller Object, Attribute 0x66 Amplifier Status is…
Modbus Poll is a useful software tool for testing Modbus RTU and Modbus TCP communication. Modbus Poll is a Modbus master that has read and write functions and has the capability of capturing communication traces. The software can be used…