This article will help you understand the differences between older S700 (S701-724) drives with single-channel STO and newer dual-channel STO S700 drives.
The PxMM can work with data from an external or shared drive. Mounting is the software process in the PxMM that enables it to read and write data to/from a shared drive. If the mounting process fails in the PxMM the following message will appear in…
Document to connect and run a F40 series Pac-Sci servo motor on the AKD drive. Note PDF below for downloading.
1. Select Feedback type 40, resolver.
a. Verify position feedback poles = 2
b. Verify transformation ratio is 0.50
2. Wire…
This application guide provides the user details with the objective of successfully getting the KBM frameless motor to commutate correctly with the AKD drive.
Troubleshooting an EtherCAT network in the field is a very difficult task. KAS 2.12 offers EtherCAT diagnostic features to help the machine builders create their machine with a diagnostic tool built in KAS 2.12 provides…
S700 and S300 Series Drive Connections for the Incremental Encoder Feedback Goldline Series Motors
This article describes the Goldline motors' incremental encoder feedback connections and Goldline motors' power connections to the S700 and the…