DESINA is an abbreviation for DistributEd and Standardised INstAllation technology for machine tools and manufacturing systems. DESINA is a specification for standardizing electric, hydraulic and pneumatic components and their interconnection on one…
Automation has placed additional requirements on cable design. These applications typically require motion. Stationary applications do not require the added stress of cable motion. When designing a cable for motion, you must consider:
Voltage rating for cables varies between standards. Typical voltage ratings for cables are 300V and 600V.
CE requires the equipment or other installations to have insulation rating equal to the maximum circuit voltage applied to any conductor within…
Valid for S400, S600
Function
For controlling several servo amplifiers, start the communication with the first amplifier via RS232 and all other amplifiers via the CAN bus. Presumption for that is, that the CAN baud rates are…