In cases where the cable length is >500mm or there are high level EMC requirements, observe the notes given below.
Connection
Use a shielded cable for DC-Bus link connection. The shield should be connected on both ends. The wires for…
The DDL catalog shows a dynamic bend radius of 15X the cable diameter for the MxC, TxC, HxC cables. The static bend radius for these cables would be 10X the cable diameter. It is important note as stated in the DDL catalog, the…
Kollmorgen does not offer mating connectors or cables for the feedback system with DRIVE-CLiQ Interface. Please use Standard cables recommended by Siemens.
M12 Connector Pinout (built into the motor)
Encoder (Feedback codes MA, MB)
The AKD's X11 Service Port is a standard 10/100 Base Ethernet port. AKD will auto-negotiate the bit rate and supports full-duplex mode only. Unplugging and reconnecting the cable signals the drive to auto-negotiate again (so at…