An AKM motor with resolver can be operated with an SC900 series amplifier providing that the motor is within the current limitations of the drive. Typically the motor resolver offset must be set to 240. This is in the configuration screen and called…
The following provides brief explanations of the most important points for AKD commissioning and also goes into more detail on the key issues which need to be taken into account:
Basic settings of the AKD
Before the first controller parameters are…
Valid for S300, S400, S600, S700
Resolution in the position loop must be set precisely for linear applications or gearing with rotary appliaction to get a simple positioning with SI units.
You can setup the resolution with the setup…